This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82864A: Current Limit

Part Number: TPSM82864A

Hello,

The TPSM82864A datasheet shows different high-side and low-side current limits as shown below.

What is the current limit value of the TPSM82864A power module when the customer uses it?

Thank you.

  • Hi,

    The different current limit specifications and their use are explained in section 8.3.6.  

    Was that your question?

    Thanks,

    Chris

  • Hi Chris,

    Thanks for your reply.

    Could you please give us the exact current limit value based on the output load current ?

    Thank you.

  • Hi,

    I'm not sure that I understand your question.  The TPSM82864A does not limit the output current directly, but limits the inductor current.  The corresponding output current limit must be calculated.

    The output current at which the device reaches current limit is when the peak inductor current reaches the high-side FET current limit value.  This is when the output load current = the high-side FET current limit - 1/2 of the ripple current.

    Does that help?

    Chris