Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73605-Q1: Efficiency

Part Number: LM73605-Q1
Other Parts Discussed in Thread: LM73606, LM73605

Hello, 

I have a small doubt, please clarify.

I'm referring to the datasheet of LM7360x-Q1 from TI website for accurate efficiencies of LM73605 & LM73606 at Vin = 12V, I(Load) = 2A  & Vout = 5V
 

Here i can see that efficiency for LM73605 and LM73606 is 97% and 96% respectively. Are the efficiencies which I mentioned are correct?

Please mention the accurate efficiencies for LM73605 and LM73606 if they were wrong.

  
Thank You