Hello there,
Me and my team have designed a flyback supply based on the UCC2871x Controller. The supply is supposed to deliver 36V (main/controlled winding), and 12V from an additional winding. The output power is approximately 35W.
The rectified DC voltage is ~565V.
While testing with ~220Ohms connected at the 36V output and minimal load at the 12V I experience the following:
- The controlled RMS voltage is approximately 30V and behaves as in the attached waveforms. The ripple is high and it seems that the duty cycle varies wildly.
- The 12V appears to be well regulated, since there is an LDO.
Could you help me identify the issue with the design?
All the best, `
Georgios