This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2521: Pin handling when EN/UVLO is not used

Part Number: TPS2521

Hello,

I would like to ask about the pin handling when not using the EN/UVLO of the TPS2521.
I am thinking of using only the internal UVP (2.53V typ) of the device without using the EN/UVLO function.
If so, what should I do with the EN/UVLO pin?
Can I connect directly to the IN pin?

Best regards,