Other Parts Discussed in Thread: TPS650861
Hi Experts
do you think TPS65916 is proper solution for MP5496 ?
base on supply and performance?
BRs
brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
TPS65916 may be fine solution for MP5496 based on supply and performance. Only difference is MP5496 looks like it may have 2 bucks with 4A+. We also have the TPS650861 and the LP8756x that can reach 4A, but may not meet the other requirements. As example, the LP8756x will not have the LDO's that are similarly seen in theTPS65916 and MP5496. If the end application can work with the levels provided by the TPS65916, then it should be a fine solution.
Thanks,
Field