Other Parts Discussed in Thread: TPS55288, , TPS65987, PMP40801, TPS65982, TPS65987D, LM3489
Now that I have the utility TPS6598x Application Customization Tool communicating to the TUSB546EVM via I2C, my next step is to understand how to interface it with the TPS55288EVM. I have seen that this is done with a later version of the power path part: TPS65987 and the TPS55288 with the PMP40801, which I cannot order, but would need to be built. The issue I am having is understanding the steps needed to add support for the power supply to the binary image for this EVM if it is even supported. Is this performed with the utility and how? I am not seeing anything obvious when starting a new project using a template with the TPS65982 or the TPS65987.
Is there some documentation that would provide some more detail on how to do this?
The plan is to use the following parts together:
DisplayPort/USBC Multiplexer: TUSB546AI
Power Path Controller: TPS65987DDH
USB Power Supply: TPS55288
For a dual-role USB-C connector and both be powered by the USBC port (Sink for charging an internal battery) and deliver power to an external device (source) like a smaller Display Port monitor,
Thanks for any tips.