Other Parts Discussed in Thread: BQSTUDIO
Hello,
Looking at the two reference designs in the datasheet (figures 19 and 20 respectively) I'm wondering if there is some reason the RC2 pin is not connected in the i2c design? Is the intent that firmware should be polling this chip regularly, such that an interrupt pin is not required? If I do chose to use it as an interrupt pin using i2c and not HDQ, what kind of resistance should I put on the pin and to where (REG25? GND?) if I am planning to connect it to a GPIO on a microcontroller elsewhere? Is this pin normally held low and interrupt signaled by it pulling high or the opposite? Also what is the pulled up voltage? Is it the 2.5V regulator voltage? That'd be my guess from the Functional Block Diagram but I'd like confirmation.
Best regards,
Christopher