Hello,
I am using several TLVM23625 in my design.
19V input->5V output
19V input->3.3V output
19V input->1.8V output
19V input->1.2V output
19V input->1V output
5V input->3.3V output
5V input->1.8V output
5V input->1.2V output
5V input->1V output
I need to know the efficiency (depending on load current) of each supply chain above, but in the datasheet I only have 12V/24V/36V input voltages.
Does TI has efficiency calculator or some other method to calculate the efficiency?
Thank you.