Hi,
Alternate part is required for LM2675MX-5.0/NOPB.
Regards,
Vivek
Thermo Fisher Scientific
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Alternate part is required for LM2675MX-5.0/NOPB.
Regards,
Vivek
Thermo Fisher Scientific
Hi Vivek,
What's the maximum input voltage for this application? Can you use a 36V part, if so I recommend one of these:

Thanks,
Andrew
Hi Andrew,
Thanks for your response.
Vin = 12V+/-10%
Vout = 5V
Iout = 1A max
Fsw < 250 KHz (To reduce EMC issues).
Controller must have internal MOSFET.
Pin to Pin compatible will be better if possible or with minor modification.
Better to connect some person from India, so that query can be resolved as soon as possible.
Regards,
Vivek Agarwal
Hi Vivek,
TPS5410-EP is pin to pin (for HSOIC - 8), but it's switching frequency is fixed at 500kHz. I don't think we have anything else with the exact pinnout that you have. The good news is that the FB voltage is the same, so you won't have to modify the feedback resistor network.
How flexible are you on the pinnout? Are you more comfortable with modifying the design for a different pinnout, or a different switching frequency.
https://www.ti.com/product/TPS5410
Thanks,
Andrew