Hey team,
Real quick question on the UCC27710 - there are no specific startup conditions that the customer has to satisfy, correct? It seems that the biggest concern / hold-up for start-up will be the UVLO triggering on VDD/VSS and HB/HS. That being said, this is all handled internally to the part so assuming VDD > Vdd,on and ~>50us has passed, HO/LO will be switching as expected in conjunction with HI/LI? (as per figure 30 in the datasheet)
Thanks,
Cam