This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A14: How to program TPS7A14 for 0.6 V output?

Part Number: TPS7A14
Other Parts Discussed in Thread: TPS7A10, TPS7A11

Page 1 of the TPS7A14 datasheet says:

Available in fixed-output voltages:
– 0.5 V to 2.05 V (in 25-mV steps)

However table 11.1.2 describes the device nomenclature as TPS7A14xx where xx is the nominal output voltage. Using this nomenclature the lowest voltage TPS7A14 available as an orderable part is TPS71A1408PYBKR i.e. 0.8 V output.

We need a 0.6 V output. We reached out to customer support and were told:

The TPS7A14 is capable of being programmed to output 0.6V. Having said that, please reach out to our product applications specialist, as this is a special request and there are other things we have to evaluate.  

Please can you help us understand how we can get a version of the TPS7A14 that supplies 0.6V output?

Thanks

John