This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561-R1: test accuracy

Part Number: BQ27Z561-R1

dear

     The ChemID used before is # 7153, because the accuracy error has been large, there is no improvement plan, now we upload the data to the official website, re-match the ID5677, test accuracy is greater, however, the RSOC can not be fully charged, always keep 99% , such as the attachment GG file and the test of the original LOG, what needs to be done to display 100% ;

   2. In addition, can TI engineer explain how the Cell 1chg Voltage at EOC value can be set properly, whether the battery will update itself during use, and what are the conditions for updating? Because my current project has two batteries, another project is also set to 4446 mv, but after doing the learning cycle, this value has become 4339 MV, and this can not charge the meter this value, after doing 4 cycles, there is still no change

any advice?thanks in advance~