Part Number: TPS2062
hi Team,
OEMs wants to project the voltage input to the battery pack.
the abs max voltage for the pack+ pin is 30V, they concern that externally might have 48V from the adaptor if the front end malfunction
the maximum current that can go in to the battery pack is ~12A.
can you please help recommend a suitable device to prevent over-voltage event?
appreciate the help