Other Parts Discussed in Thread: CSD87334Q3D, CSD87351Q5D
Hello there,
We planned to use the Boost controller "TPS43060" in our project, and for that, we have selected the FETs based on the FET selection sheet. Could you please confirm that the selected FETs can be used for our requirements listed below?
Requirements,
1. Ambient temperature : -20 to 65 Degrees,
2. Input Voltage : 7 to 17V
3. Output voltage : 19V
4. Load current : 5.5 to 6A,
Selected FETs. (will choose one of FET )
1. CSD87334Q3D
2. CSD87351Q5D
Thanks