Other Parts Discussed in Thread: LMR51420, TPS62932, TPS62933, TPS62933EVM, TPS54202
Can you help please with the drop out in our case for a 11.38V in, what output can we set for at 1A ?
Comparing
TI LMR54410DBVR (45V, 1A, 1.1MHz FPWM, SOT23-6 (2.9x1.6mm), Sync, 240mR) (P2P with LMR14010A 1A Sync, or LMR50410 1A Sync
To Diodes AP632000 (32V, 2A, 500KHz FPWM, TSOT26 (3.0x2.8mm), Sync, 125mR)
Yes, I know its 1A vs 2A
BUT, Dropout is a consideration
We have 12V AC supply, through a Bridge of 2 x MBR230S1F-7 = 0.31V @1A, so Vin is 11.38V
LMR54410DBVR dropout seems to be 0.7V @ 1A
So if we add a LMR54410DBVR 0.7V, we have effective Vrail of 11.38-0.7= 10.68V
TI graphe here: vs Diodes
Diodes AP632000 Below seems to suggest that we would have 5.18V out for a 5.0V in ? so no dropout at all ?