Other Parts Discussed in Thread: LM5149
Hi Ti,
i plan to use the LM5149-Q1 for a 48V Vin and 12V 6A out DC/DC Buck Controller. Because of my limited space and the much higher switching loss of traditional Fets im considering using GAN Fets for at least the upper MOS Fets which genereates the higher switching loss, but also the lower one is maybe better a GAN Fet due to no reverse recovery loss. I see the Gates are driven by the VCC which is 5V only so my GAN Fets with 6V Vgs should be OK. Is there any point that I dont see so far which makes it impossible to use GAN Fets instead of Silicium Fets with this controller?
Thanks in advance
Marcel