Hi,
The power supply circuit is designed using TPS54332DDA.
24V input, 12.8V output, as shown in WEBENCH on TI's website, The circuit was configured with the constants of the peripheral elements confirmed by WEBENCH on the TI website.
Then, at an output of about 1A, a drop in output voltage and oscillation-like behavior were observed.The circuit configuration is shown in the attached PDF file "DCDC initial circuit" and the peripheral components are replaced with "WEBENCH_2A circuit" for confirmation. The rising waveform with a resistive load is also attached.
Any comments on the cause of this phenomenon would be appreciated.
7367.Schematic.pdf
Thnaks,