1.I want to confirm that does the input voltage (5V) from the power source should exceed 2.95V (UVLO START THRESHOLD VOLTAGE) within or equal to 2.5us(rise time) to turn on the device or else will it go to shutdown mode and if t is confirm then is it possible that the power source slow rise time mismatch from the IC rise time to operate the device will it make the IC to shutdown and how to solve it?
2. Is it possible that the power source rise time mismatch from the IC UVLO start up threshold rise time and does it make any problem to get the output ?