This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25149: Using same MOSFET for high-site and low-site

Part Number: LM25149
Other Parts Discussed in Thread: CSD18514Q5A, CSD18504Q5A, LM5148

I'm making a design with LM25149

Design spec.: 15V to 28V input and 12V output, max current is 7.5A

I have used Webench for a design suggestion.
Webench suggest CSD18504Q5A for high-site FET and CSD18514Q5A for low-site FET
If I try to select an alternate part I can only select deferent FET´s for low and high-site
Is it not possible to use CSD18514Q5A for both FET´s?

Thanks in advance
/Gert