This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM846C24: Vias on Footprint questions and AGND/PGND connection

Genius 3890 points
Part Number: TPSM846C24

Hi there, We use TPSM846C24  to convert 5V to 0.95V, 25A.

Some question to consult. Thanks !

1. Could you help provide TPSM846C24 footprint files , we use allegro 16.6. The download file from product page seem not usable.

2. There are many vias resident right on the pin pads(as I marked out in blue rectangle ) ,I understand this is for thermal and current density, but from SMT process perspective, we generally DO NOT do this "vias in pad". How do you think?

3. There are also dashed-line vias (as I marked with red cycle), some of these via are rather close to pin pad, we tend to remove them to avoid possible short. How do you think?

4. I assume the locations of all those vias are recommending, we can adjust them .

5. AGND and PGND are internally connected. How should we connect them on PCB board?  Our PCB has >10 layers, we plan to use a small area of copper as AGND under the IC, and connect it to larger PGND layers with single point connection (maybe through a 0 ohm resistor). How do you think?