This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25898: Current drop and different terminal current in different IR compensation

Part Number: BQ25898

Hi team,

Our customer they are using BQ25898 in there mp product. But the met some problem. Could you please help to analyze why the current will drop suddenly when approaching the end of charging and why the terminal current is not aligned with the setting value 192mA? Thanks!

After setting the BAT_COMP to 140mR and VCLAMP=32mV, the actual voltage of the battery can be charged to 4.4V, but the charging terminal current stops when it reaches 500mA, and the charge IC register is read
A cut-off current of 192mA can be seen.

com8_multi_2023_07_25_16_38_31(1).csv

Set BAT_COMP=20mR40mR The following phenomena occur, when BAT_COMP=20mR, the charging will be switched around 2A, the current will suddenly drop to 1.4A, and finally complete the charge, the terminal current is 230mA.

BAT _COMP=40mR, the charging will be switched around 1A, the current will suddenly drop to about 500mA, and finally complete the charge, the terminal current is 230mA.

IR=20mA-488.csvIR=40mR-488.csv