Part Number: BQ25628EVM
Other Parts Discussed in Thread: BQ25628
In Boost Mode Load Transient test (VBAT = 3.8 V VBOOST = 5.04 V IBOOST from 5 mA to 500 mA), the maximum voltage of PMID is 5.54V and the minimum voltage of PMID is 4.76V, is this satisfied standard? Is there a risk of triggering PMID-OVP (MIN 5.5V)?