This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ATL431LI-Q1: application information

Part Number: ATL431LI-Q1
Other Parts Discussed in Thread: TL431, ATL431LI

Hi Expert, 

Customer refer to below example for ATL431LI-Q1 to design a 50mA output capability circuit. But do you have any recommendation for system workarounds to protect 2N22 not damaged when overcurrent and short circuit events happen? 

Thanks!

Ethan Wen

  • Hi Ethan 

    • This circuit is not recommended for the application where user is expecting short circuit at VO because of some other source. (stratup is not included in it)
    • You can use the circuit described in section 10-7 of TL431  data sheet. 

    Can you please explain bit more about the application and tell  

    • the expected output voltage 
    • if there is continious load current or user will be switching it and
    • if the short circuit only comes at the startup or there is any other short circuit condition? 

    I'd recommend to use TL431 for 50mA current application. Why ATL431LI has been chosen ? 

    Regards 

    Trailokya 

  • Hi Trailokya

    I am the senior hardware engineer from KOSTAL China, and Ethan is our support FAE.

    According to your question, let me explain more details about them.

    • the expected output voltage  --- 5V
    • if there is continious load current or user will be switching it --- We use it as LDO on board and should not switched off, the maximum load current 50mA
    • if the short circuit only comes at the startup or there is any other short circuit condition? --- Not for startup beacuse no large bulk capacitor on the output, we just worried if output short to ground on board, the darlington transistor would be burned because there is no short current protection.

    We use ATL431LI as LDO output due to its low quiesent current, 80uA maximum in cathode current. As a contrast, 1mA in cathode current for TL431.

    If using the circuit that you mentioned, for example, 50mA output capability, in sleep mode, the quiesent current is still 50mA.

    That's why we use the combination of ATA431LI and darlingtion transistor. It is better if there has darlingtion protecion in case short current happened. 

  • Hi Qilong 

    Thanks for clarification. Can you please tell me the supply voltage. Is it a DC DC or battery.   I have couple of comments 

    • The easiest sollution (with some performance limitation) will be to add a seriese resistor (R2 as shown in the figure) from supply 

    This method can be used only when  below condition satisfies

    V(BAT)/ (MAX_IC_BJT ) < Rs < 80mA  

    I have given 30 mA margin. You can tweek the variation. 

    • Other solutions require couple of transistors and stability gets challanging in discreet implementation. 

    Can I ask what is the reason you are not using a crude LDO at this stage ? Is it cost or any other reason? 

    Regards

    Trailokya 

  • Hi Trailokya,

    Thanks for your serveral solutions.

    As you mentioned, It is a battery supply voltage, if add a series resistor between supply and darlington, R2 power consumption is much higher in case Vout short to ground.

    For example, VBAT is 9-16v, Vout is 5V and minmum 50mA output current, the saturation of dalington transistor is ~1.4V dropout, so maximum R2= (9-5-1.4)/50mA= 52ohm.

    If Vout is short to ground, in the worst case VBAT is 16V, the power consumption R2= (16-1.4)*(16-1.4)/52= 4.1W.

    It is hard for us to control the base current of darlington transistor accurately to limit the maximum output current beacuse the hfe gain of darlington transistor is at lease 6000~10000 typical.

    The reason we use discret component beacase it is a backup power supply on board, and certainly the cost of crude LDO is expensive than ATL431LI. So the crude LDO is our alternative.

    I am interested in your second comment, how to implemente the protection with couple of transistors?

  • Hi Quliong 

    Below circuilt will restrict the current 

    You can tweek resistor R11 to adjust max current in your circuit. 

    You can also compare the cost of this solution with UA78M05QDCYRG4Q1 LDO. Let me know if you have furter question.

    Regards

    Trailokya 

  • Hi Trailokya,

    That's ok, thank you for your support.