Other Parts Discussed in Thread: BQ77216
Hey Guys,
I'm having difficulties pairing bq77915 with bq77216 for LFP chemistry
i thought of pairing bq7791514 (3.65V OVP) with bq7721611 (3.8V OVP), but it seems that bq7791514 has been discontinued.
if i go with bq7791506 instead (3.8V OVP) then bq7721611 (3.8V OVP) could trigger the fuse during regular use and bq7721614 (3.9V OVP) seems unavailable too
A. Is the 3.8V OVP of bq7791506 safe instead of 3.65V for LFP ?
B. pls suggest a suitable combination or an alternative for this scenario
C. what about the bq769X2 ? are there any reference designs that doesn't use a microcontroller ?
appreciate the help
thanks & Regards