This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5140-Q1: LM5140 VDDA pin

Part Number: LM5140-Q1

Hi,

Vin=12V Vout1=3.3V Vout2=5V 

Since our outputs are 3.3V and 5V, we connected the FB pins as follows. But when we take measurements, we can't see 5V on the VDDA pin, so the outputs are not as we expected. What could be the reason for this?

Best regards.