If the Vin voltage is 3.3V, can 5V be applied to the enable pin? In the datasheet, it specifies an absolute maximum voltage on each of these pins as 6V, but does not clarify whether the IC can handle up to that 6V on the enable pin if the VIN pin is a lower voltage like 3.3V.
Thank you!