The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: TLV62130RGTR does not work

Part Number: TLV62130

Hi  I use TLV62130RGTR to generate 1.8V and 1.0V power as picture 1 and picture 2 show. there two schematic are the same.

for 1.0V power, it works normally.

for 1.8V power, it does not work.

for 1.8V power,  what i did as below

1). Pull up EN pin to 5V and disconnect R1112, 1.8V power does not work.

2). disconnect  both  R416 and inductance L19, and then I test circuit after the chip TLV62130RGTR ,  the circuit after the chip TLV62130RGTR is good.

what should i do now?