Part Number: BQ7718
Hi,
Based on the BQ7718 datasheet, the typical supply current is 1uA when cell voltage is 4V.
1) What is the IC supply current if the cell voltage is 3V/2.5V/2V?
2) What is the min IC supply current if cell voltage is 4V?
Please refer to the following table. Please help to provide the values of the IC supply current for different cases.
| IC Supply Current | |||
| Cell Voltage | Min | Typ | Max |
| 2V | ? | ? | ? |
| 2.5V | ? | ? | ? |
| 3V | ? | ? | ? |
| 4V | ? | 1uA | 2uA |

Thanks,
Kim