Dear,
I would like to understand the behaviour of BQ21061 battery charger at the power up when it is connected to a protected rechargeable battery (I'm speaking about the case in which I attach power to the "IN" pin of the BQ21061 and the protection of the battery is open). As you can seen from the picture attached (yellow trace) it seems that the battery charger implements a sort of "Battery Detection" procedure with successive discharge-charge pulses before to "understand" that the battery was attached (or better to say, the battery charger with this procedure closes the protection and therefore it realizes that there is a battery connected). We noted that this sort of "Battery Detection" procedure has duration that is not standard and could persist up a few seconds. Inside the datasheet of the BQ21061 this "Battery Detection" procedure is not documented but I found the same procedure inside other Texas battery chargers. Please can you confirm that this successive pulses are due to the "Battery Detection" procedure of the BQ21061? If the answer is yes, please can you give me details (timing and charge-discharge currents) with which BQ21061 performs this procedure?
Thanks
Francesco