Hi
The customer design with BQ24295, The J20 position in the figure is connected to the battery. When is not charging (the J21 pin is not connected to an external 5V power supply), the system is turned off and there is no load connected to the BAT+ position. use the default value.
Use a multimeter to connect the positive pole of the battery to the J20-PIN1 pin (that is, BAT+ in the figure below) in series, and find that the battery has a current of 2.2mA. This leakage is too large.
How to reduce this leakage current.

Waiting for your reply.
Thanks
Star