This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ29200: BQ29200 balancing in sleep mode (not charging)

Part Number: BQ29200

Dear Team,

My customer wants to use BQ29200 in a system, where their device is spending most of the time in sleep mode. However, they have a system with a 2 cell battery, where the cells are unevenly loaded. In sleep mode the first cell has a current draw of 280uA and the second only about 11uA, which means a 30mV imbalance after some time in sleep mode.

As long as the BQ29200 is enabled by grounding the EN pin, can you confirm that the cell balancing will also happen in deployment where the end device is spending most of its time in sleep mode?

It seems that BQ29200 is a rather simple device and should always perform the balancing as long as enabled even when not charging, but please confirm.

Thanks,

Daniel