Input Voltage=15V,no load,but IQ=57mA,something is wrong,IQ should below 1mA。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Input Voltage=15V,no load,but IQ=57mA,something is wrong,IQ should below 1mA。
Hi Wenhe,
thank you for using the E2E forum.
Can you please mark in the schematic above where you are measuring the current.
What is the scope plot showing above? L wave = Switch node (SW) ?
Note: you still have some current through the Feedback divider and the leakage of the Capacitor.
Depending on that you will see pulse skipping
Best regards,
Stefan
Hi Wenhe,
So the question is:
why is the current higher the 1mA?
or why do you see switching on the Switch node?
Pulse skipping starts when the output voltage is still to high when the next switching cycle starts.
As long as the output side is consuming energy more then with the minimum duty cycle does deliver on Energy, no pulse skipping is required.
Load on the output is the some of: load, current through Feedback resistor divider, output cap leakage.
Best regards,
Stefan