This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS785-Q1: TPS78508BQWDRBRQ1

Part Number: TPS785-Q1

We are facing issue in TPS78508BQWDRBRQ1 LDO We have require 2.5V output for this circuit but we get 0.8V.

Input Voltage: 5V
require current : 50mA

  • Hi Haresh,

    The part number you have listed is a fixed 0.8V output.  The "08" in the part number is the output voltage.  You want the "25" here to get the same device in a 2.5V output.  This is the part number you should be ordering:

    TPS78525BQWDRBRQ1

    Thanks,

    Stephen