This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: Issue with GAIN of internal differential amplifier for ACSET (IDPM)

Part Number: BQ24610

Hello, 

I was trying to set DPM current, but I think that equation (3) in datasheet is incorrect:

I set voltage Vacset to 430 mV and this should equal to current limit up to 2,15A, but real limit was only 1,7A.

or 

I set voltage Vacset to 580 mV and this should equal to current limit up to 2,9A, but real limit was only 2,3A.

I think that gain of internal differential amplifier is not 20 but is 25? It is correct?

Thank you

BR

Jakub