Hi,
I'm using a TLC5943 to drive 5 x RGB LEDs in a new design (so it uses 15 of the 16 channels).
The peak current is set to 5mA/LED, and each channel only has a single LED attached, so the LED supply is 5V.
GSCLK is 1MHz.
The chip supply is 3.3V, and I'm trying to understand the datasheet specs on Icc so I can verify my power budget.
From the datasheet, it appears that Icc
a) depends on the peak LED current programmed by I(Rref)
b) depends on the frequency of GSCLK.
c) the dependency on GSCLK is also affected by the programmed Iref
The power budget is tight, and based on the numbers in the datasheet I had budgeted for about 10mA Icc when running at 10MHz GSCLK and 10mA per LED.
Obviously I'm not running it at this point any more, but the actual measured Icc is significantly lower (~1mA), and also doesn't seem to vary much as I change GSCLK from 100kHz - 5MHz.
Can someone explain :
- how Icc should vary with the LED reference current (and why)
- how Icc should vary GSCLK (and why)
- why Icc at a given GSCLK frequency also depends on Iref
Thanks.
Nick