Other Parts Discussed in Thread: UC1843BEVM-CVAL, UC1901, UC1843-SP, UC1843, UC1843B-SP
Hello,
I am designing a power supply using the UC1901-SP for isolated feedback. In the reference design for the 'UC1843BEVM-CVAL' eval board, a 2.5V offset it added to the feedback signal by using the UC1843B's 5V reference and dividing it down using two 2.74k resistors:
My understanding is this 2.5V offset is needed because the UC1843B uses a 2.5V reference for its feedback and the UC1901-SP output capability is limited to 1.5V max. Is this correct?
If I want to simplify my circuit and avoid the need for a 2.5V offset, can I use a 1:2 transformer instead in order to increase the range to 3.0V (2 x 1.5V), so that I exceed the 2.5V reference? If so, any drawbacks?
If I decide to not use the UC1843B and instead use a controller with a 1.2V reference, can I do away with the offset and connect the feedback signal (post-diode) to my controller?
Thanks!