Part Number: TPS23880
Other Parts Discussed in Thread: TPS23755, TPS23753A
Hi team,
Could you please kindly help recommend a device?
Requirements:
- Front connect with Marvell 88e151x PHY
- Back connect CAT5e cable
- 48V DC
Thanks,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
How many ports will be supported and what is the power level needed for each port?
Regards,
Brandon
Hi Brandon,
They only need the PD device of POE.
1 PORT,12.95W
PoE IEEE 802.3af (802.3at Type 1) Class 3 (nom. 48V DC)
Power consumption up to 12.95W (PoE class III)
Small size is better.
Thanks,
Brian
Hi Brian,
Is isolation needed and what is the output of DCDC converter? Will customer need primary or secondary regulation?
Regards,
Brandon
Hi Brandon,
Others beyond the requirements are all not needed.
The output is not defined, they only want us to recommend a device now for them to have a look.
Thanks,
Brian
Hi Brian,
The device recommendation would be based on those considerations as our devices have slight differences which allows them to perform to the application. For class 3 power I would recommend TPS23753A or TPS23755/8.
Regards,
Brandon