Hello,
We are implementing the TPS7A57 as follows: https://imgur.com/RVTk2RR
I measure the output voltage as 2.1V when our reference from the DAC MCP4728 is 0.93V. We have shorted the bias and input voltage to 3.3V although it doesn't matter the internal circuit should use the 3.3V input voltage as no bias is needed (I have tried enabling and disabling the CP with J105). Why is the output voltage 2.1V when we expect 0.93V as defined by the reference?
Appreciate your feedback.
Thank you!
Arnav