Part Number: TPS2412
Datasheet recommend the minimum Rset is 1.5k ohm. Since our design need a huge threshold, so we change the Rset to 0.51k ohm. May I know that have any impact?
BR, Gary
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gary,
As you mentioned, Rset = 0.51 kohm resistor is out of recommended range (1.5kohm to open is recommended) and hence the TPS2412 behavior for this resistor is not characterized. This means the reverse current threshold accuracy may be very poor as a low value Rset resistor is used.
Also,. the reverse threshold setting with Rset = 0.51 kohm resistor will push the reverse cutoff threshold close to ~ -921 mV which means huge reverse current needs to flow to turn off during reverse current. It doesn't damage the TPS2142 device as the operating voltage will still be within the absolute maximum range.