Part Number: BQ24195L
Other Parts Discussed in Thread: BQ24195
I have designed a circuit with BQ24195L that will not charge. System pin outputs about 4.1V when VIN is 13.5V, and drops to Li-Ion (3.7V) when 13.5V is disconnected, so it's at least doing something.
I have followed the Typical Application on page 34 of the datasheet, but omitted Q1/Q2 circuit, Q3/R11. OTG is not used and floating.
Inductor is a 2.2uH (3.3A, 68mOhms DCR).
NTC 10k with 5.6k/33k resistors.
I feed it with 13.5V and have a single cell connected. Charge enable is pulled low.
I have read all the registers and see all conditions are ok, for example REG01[5:4] = 01. Watchdog kicks in after some time.
I also see the battery is fed (charged?) 82mA, but in pulses. Cycles between 82mAfor around 2-3 second, then drops to 0mA for a few seconds.
Do I have to set / start something at first time use? Or could the pulsing be a sign that the buck can't start properly (DRC or other spec of the inductor not compatible with bq24195 spec)?