This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Usage with variable input/output for amplifiers

Part Number: TPS25982
Other Parts Discussed in Thread: TAS5825P

Hi:)

-

Can the TPS25982 be used in a variable input/output setup?

Specifically, I intend to use this part at the output of a boost converter, which can vary its output from 9.4 V to 18.4 V (approximately 1.2 ms rise time from min to max) with 16 voltage steps using of the TAS5825P Hybrid-Pro feature.

-

Thanks!