Hi.
Let's talk about the input current limit setting.
I have two questions.
1.
IINLIM values of "page 28" and "page 34" in the datasheet are different.
Which is the correct value?
Page28:3.25A / Page34:3.15A
2.
Customer has tested IINLIM.
The difference between the measured value and the set value was about 100mA.
Could you tell me the offset guideline for REG00 register?
REG00 | IINLIM | Measurement result | ||
0x00 | 0 | mA | 93.7 | mA |
0x01 | 50 | mA | 143 | mA |
0x02 | 100 | mA | 190 | mA |
0x03 | 150 | mA | 239 | mA |
0x04 | 200 | mA | 287 | mA |
0x05 | 250 | mA | 331 | mA |
0x06 | 300 | mA | 378 | mA |
0x07 | 350 | mA | 426 | mA |
0x0A | 500 | mA | 561 | mA |
Best regards,
Yusuke