This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988DK: GPIO configuration and HW register anomaly

Part Number: TPS65988DK

Hi!

I tried to set GPIO14 and 15 alternate function to PWM with Application configuration tool (6.1.4) via DH advanced setting with swapped FW. But when I uploaded that on the IC GPIO configuration (0x5c) is incorrect.

Raw value of register 0x5c in App conf  0x9001200000000000000032729000000002a0000000000000000000000000003c0080000000000000000000000000002b0e7 where MUX select bytes 17-20 with value 0x000003c0 doesn't switch gpio14 and 15 to alternate function.

Running that generated binary GPIO 14 is input and GPIO15 is output with attached event SourcePDO0ContractBit0_Port2.

Another thing to note Host Interface Technical Reference Manual says that HW control register (0x6b) is 9 bytes, in App conf it is 12 bytes, but actually reading that register says that it is 10 bytes in size.