In trying to use this model with in a simulator I am encountering errors related to the following SPICE declarations
V_IRT1 RT1VAL RT1
V_IRT2 RT2VAL RT2
The simulator reports that it is expecting five parameters here when only two have been declared? This is in fact true whereas both are voltage source IDs that are lacking specific AC and DC values. Would you please correct this or send me an updated SPICE model that fixes this issue? The particular version of the model I am using is LM25037_TRANS.LIB version 1.20 dated (November 10th, 2016) as located on the part's product page and published as your unencrypted model. Thanks!