The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery pack and Charger Recommendation

Other Parts Discussed in Thread: BQ40Z50, BQ7718, BQ2962

Dears,

Please recommend 3 ICs(gas guage IC, protection IC and charger IC) for 2 new products (battery pack and charger) with main parameters:

         Battery pack: (gas guage IC, protection IC)

         Cells: 4S1P

         Charge:16.8V+/- 0.2V, 4A at 0 to 50 ℃, 0.5mA at below 0℃

         Discharge: 10A max, 6.5A continuous

         Communication interface: SMBUS

        

         Charger: (charger IC)

         Charge voltage: 16.8V+/- 0.2V

         MAX Battery Charge Current: 0.5mA < 0C (MAX) , 0C < 4A < 50C

         Communication interface: SMBUS