Other Parts Discussed in Thread: TPSM82810, TPSM82864A,
Good day,
I see that Buck converters like the TPSM82810 is rated for a Maximum Effective Output Capacitance of 470uF and the TPSM82864A datasheet states that Effective Output Capacitance "Values over 150 µF can degrade the loop stability of the converter."
Does the TLVM13640 have any restrictions in terms of the maximum effective capacitive loads that it can drive? I do not see any related information like this in the datasheet.
Thanks.