I want to check if my BQ79606Q1-EVM is working or not , then how would i know if its powering on ?
does it have any in built led on it ?
or any other way to test if this evm is working or not?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to check if my BQ79606Q1-EVM is working or not , then how would i know if its powering on ?
does it have any in built led on it ?
or any other way to test if this evm is working or not?
Hi Akshay,
The BQ79606Q1-EVM has a LED, D1, that will light green when the device is woken up. An additional LED, D2, will light up when J17 is populated and the device is woken up. You can also probe AVDD and GND and the voltage will typically be 5V±0.1V if the device is on.
Regards,
Ben