Hi Team:
I want to use one pin to indicate OCP, OVP, UVP, OTP and power good, so should I connect PG and FLT together to achieve this function?
Or use a diode between PGTH and FLT like in the picture I pasted? THANK YOU.
In addition, I need to combine two parallel tps26630's Imon signals into a single IMON pin to FPGA, how can I calculate the appropriate Rimon? The maximum current of the system is 5A
THANK YOU.