Other Parts Discussed in Thread: LMR50410, LMR51610
Hi support team,
What are the main differences between LMR54010 and LMR54410?
I found below.
| LMR54010 | LMR54410 | |
| VIN Abs (MAX) | 38V | 45V |
| SW to GND less than 10-ns transients Abs | -3.5~38V | ? |
| Output voltage (MIN) | 1V | 0.8V |
| SWITCHING FREQUENCY | 700kHz | 1.1MHz |
| VOLTAGE REFERENCE | 1V | 0.8V |
| FB pin voltage required to trip short-circuit hiccup mode | 0.4V | 0.325V |
Does LMR54410 have a "SW to GND less than 10-ns transients" specification?
Regards,
Dice-K