This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1117: Thermal Calculations

Part Number: TLV1117

The datasheet provides thermal metrics but there is no guidance on how to use them for this particular device. It references the TI Semiconductor and IC Package Thermal Metrics, which is primarily concerned with measurements. I though I knew how to do the thermal calculations but I need some helpful guidance for this one.

How do I determine if my design will work? I know that the thermal performance depends on the PCB but I'm looking at a 4-layer design with 2S2P layers where there are many small vias that connect the layers around the device. Assume the PCB is a standard 2S2P setup.

In my application, the input voltage is 8.8 V and the output is 3.3 V. The load current is 200 mA. Will this device work where the ambient temperature is 85 deg. C? If not, what is the maximum temperature?

Any advice would be appreciated.

Whit